What happens when a CRAC unit controller reaches end of life?
When the controller becomes the weak point
A CRAC unit can still be in good mechanical condition, but that does not necessarily mean every part of the system is equally reliable.
While compressors, fans, and heat exchangers often receive most of the attention during maintenance, the controller plays an equally important role. It manages unit operation, regulates temperature and humidity, monitors operating conditions, and signals alarms when something is wrong.
Like any electronic component, controllers have a limited lifecycle. As they age, the risk of electronic failure increases. At the same time, older hardware and firmware can become harder to maintain, repair, or replace.
The challenge is that these issues are not always visible during normal operation. A controller may continue working for years without any noticeable problems, until a component fails or replacement parts are no longer available.
Why controller age matters
For CRAC units that have been operating for 15 years or more, controller lifecycle deserves particular attention.
Even when the cooling equipment itself remains operational, an aging controller can introduce risks that affect the entire unit.
These include:
- Loss of unit control
A controller failure can prevent the CRAC unit from operating correctly or stop it altogether. Unlike the failure of an individual sensor or peripheral component, a complete controller failure may result in the loss of the entire unit.
- Reduced control over temperature and humidity
The controller is responsible for maintaining the required environmental conditions. If it fails or develops faults, the unit may no longer be able to regulate temperature, humidity, or other operating parameters as intended.
- Increased risk of electronic failure
Electronic components deteriorate over time. Aging circuit boards, connections, and internal components can become more susceptible to faults, particularly after years of continuous operation.
- Hardware and firmware obsolescence
As technology develops, older controllers may no longer be supported by the manufacturer. Firmware updates, replacement components and technical assistance can become increasingly difficult to obtain.
- Limited availability of spare parts
Even a relatively minor controller failure can become a major issue when replacement parts are no longer readily available. What might once have been a straightforward repair can turn into a much more complicated intervention.
The risk of waiting until failure
In a data centre, a controller failure is not simply an inconvenience.
If a CRAC unit loses its ability to operate, the available cooling capacity is reduced. Depending on the site's redundancy strategy and operating conditions, that can put additional pressure on the remaining units.
The consequences can extend beyond the immediate loss of cooling. When a controller is obsolete, sourcing compatible replacement parts may take longer than expected. In some cases, an emergency controller upgrade may be the only practical option.
That introduces additional cost, operational disruption, and potentially longer downtime.
The important distinction is that an aging controller does not necessarily need replacing because it has already developed a fault. It may need attention because the consequences of a future failure are becoming harder to manage.
Planning controller replacement
Controller replacement is primarily a risk mitigation measure. Unlike certain fan upgrades, which may also improve energy efficiency or airflow performance, replacing an aging controller mainly maintains reliable operation and reduces the risk of unexpected downtime. For installations approaching or exceeding 15 years of operation, it is worth reviewing the controller lifecycle before support or spare parts availability becomes a problem.
This does not automatically mean every controller needs immediate replacement. The right approach depends on the controller type, manufacturer support, availability of compatible upgrades, and the site's redundancy requirements. A planned approach also allows you to phase replacements across multiple units, rather than carrying out emergency work after a failure.
The STULZ approach
STULZ can help assess the condition and lifecycle status of existing CRAC unit controllers and identify where replacement or upgrade planning may be necessary.
Depending on the installation, this can include:
- Controller identification and lifecycle review
A review of the installed controller models, their age, operating history, and current manufacturer support status.
- Spare parts and obsolescence assessment
Check the availability of replacement controllers, electronic components, and technical support to understand the risks of continued operation.
- Compatibility and upgrade assessment
Where controllers are approaching or have reached end of life, STULZ can review the available replacement options and assess compatibility with the existing cooling equipment.
- Phased replacement planning
For sites operating multiple CRAC units, controller upgrades can be planned in stages, considering operational requirements, redundancy, and maintenance windows.
- Testing and commissioning
After replacement, check the controller configuration, unit operation, temperature and humidity regulation, and alarm functions to confirm the system operates as intended.
The goal is not to replace controllers simply because they are old. The goal is to understand when aging electronics and declining support availability start to pose an unacceptable operational risk.
Don't wait for the controller to fail
A CRAC unit may still deliver the cooling capacity it was designed for, but that doesn't mean its controller will remain reliable indefinitely. As controllers age, spare-part availability and technical support can become as important as their current operating condition. Reviewing controller lifecycle before failure makes it possible to plan upgrades, manage costs, and protect cooling availability without the pressure of an unexpected breakdown.
Want to understand whether your CRAC unit controllers are approaching end of life? STULZ can review your existing installation and help identify the most suitable replacement or upgrade strategy.
More in our Cooling Practice series:
Cooling Practice 1
Why high pressure alarms return every summer.
Cooling Practice 2
Is your cooling equipment aging faster than you think?
Cooling Practice 3
Why small controller batteries can become a big cooling risk
Cooling Practice 4
Are your EC fans still delivering the airflow you designed for?