Are your EC fans still delivering the airflow you designed for?

When fan performance starts to change

In critical cooling, airflow is everything.

Fans move the right volume of air through the unit, across the heat exchanger, and into the space that needs protection. When airflow changes, the entire cooling system's performance can suffer.

EC fans are efficient, controllable and widely used in modern CRAC and CRAH equipment. But like any mechanical component, they are not immune to aging. Over time, bearings, electronics, impellers and motor assemblies can all be affected by operating hours, environmental conditions and how hard the unit has been working.

The result is not always an immediate failure. In many cases, the first sign is more subtle: reduced airflow, less stable operation, increased energy use, or a unit that needs to work harder to deliver the same cooling effect.

 

Why fan condition matters

A fan does not need to fail completely to become a problem.

If airflow drops, the unit may no longer deliver the capacity it was originally designed for. That can affect temperature control, reduce resilience, and put more pressure on other units in the room.

If the fan is worn or operating less efficiently, it may also consume more energy than expected. In larger installations, small changes in fan performance can add up quickly, especially where units run continuously.

There is also a maintenance and reliability angle. Aging fans can become more vulnerable to bearing wear, vibration, imbalance, or electrical issues. If a fan fails unexpectedly, the impact is not limited to that component. It can reduce available cooling capacity and affect the site’s redundancy strategy.

More than risk mitigation

Fan replacement is often discussed as a lifecycle or reliability measure. That is important, but it is not the full story.

For EC fans, there can also be a clear opportunity to optimize. Reviewing and, where needed, replacing aging fans can help improve airflow stability, reduce mechanical stress, and support more efficient operation.

In some cases, fan replacement is not only about preventing failure. It is also about restoring the unit to its intended performance level and ensuring the system is not using more energy than necessary to deliver the required cooling.

That makes EC fan lifecycle planning slightly different from some other replacement activities. Components such as batteries or controllers may be primarily about risk mitigation. Fans can offer both: reduced operational risk and a potential improvement in performance and energy efficiency.

What to look for

There are several signs that EC fan performance may need closer attention:

1. Reduced or unstable airflow

If airflow is lower than expected or varies more than it should, the unit may no longer deliver the designed cooling performance.

2. Increased fan speed

If fans consistently run at higher speeds to meet the same load, it may indicate the system is compensating for reduced performance elsewhere.

3. Higher energy consumption

Aging or inefficient fan operation can increase power draw, especially in systems that run continuously.

4. Noise or vibration

Changes in sound, vibration, or operating behavior can point to mechanical wear, imbalance, or bearing issues.

5. Aging beyond intended lifecycle

Even if the fan is still running, operating beyond its expected lifecycle increases the chance of failure and may reduce efficiency.

 

The STULZ approach

STULZ can help review the condition and performance of existing EC fans as part of a wider lifecycle and reliability strategy.

Depending on the installation, this can include:

1. Fan condition review

A check of fan age, operating hours, fault history, and visible signs of wear or deterioration.

2. Airflow and performance assessment

A review of whether the unit is still delivering the airflow and cooling performance expected from its original design.

3. Energy and optimization review

Where relevant, STULZ can assess whether fan operation is contributing to unnecessary energy use and whether replacement or adjustment could improve performance.

4. Lifecycle planning

If fans are approaching or exceeding their expected service life, STULZ can plan replacement in phases rather than leaving it until failure.

5. Upgrade strategy

Where a wider refresh is required, STULZ can advise on the most suitable fan replacement or upgrade route, considering performance, energy use, disruption, and long-term reliability.

The goal is not simply to replace fans because they are old. The goal is to understand whether they are still supporting the cooling strategy as intended.

We can help

Send us your inquiry to arrange a site review or discuss the most suitable next step for your installation.

Contact us directly

More in our Cooling Practice series:

Cooling Practice 1

Why high pressure alarms return every summer.

Cooling Practice 2

Is your cooling equipment aging faster than you think?

Cooling Practice 3

Why small controller batteries can become a big cooling risk